From the old to the new control system with minimised downtime

When industrial plants age, are no longer state of the art, or when support or spare parts availability is limited, a system update is required at the control level of a process plant. When replacing PLC and DCS systems, it is essential to avoid wiring errors and to keep the downtime of the plant as low as possible during the migration process. PLC or DCS migration with MiBridge from Weidmüller enables a secure exchange of the control level. Even adaptatiions or changes to the infrastructure can be performed simply and quickly without any need to intervene the field cabling.

New to the product range

Highlight

MiBridge: Replace PLC systems without minimum downtimes

Migration from Siemens ET200M/S7-300, Siemens S7-400, Rockwell SLC500

Migration of a PLC

MiBridge replaces legacy PLC systems without rewiring, minimises plant downtime and accelerated migration to modern control platforms. Using migration racks and pre-assembled cables, it connects existing and new PLCs quickly and reliably. The solution supports migrations from Siemens and Rockwell systems, including cross-vendor upgrades. By keeping field wiring in place, MiBridge simplifies modernisation, reduces project risk, lowers migration costs and helps maintain continuous operation in process and industrial applications.

  • Modernising PLCs
  • Speeding up migration
  • Avoiding downtime
  • Ensure availability

This is a YouTube video. By clicking on this video, you agree to Google/YouTube's Privacy Policy & Terms of Use . You also agree to our Privacy Policy.

Uniquely designed solution

Uniquely designed solution

The design permits your existing field wiring to remain in place and eliminates the need to wire-trace or ring-out.

Compatibility means flexibility

Compatibility means flexibility

Universal conversion/migration system for the most important PLC old systems, to migrate to any new control system.

Minimal components maximise migration efficiency

Minimal components maximise migration efficiency

Includes versions of card adaptors and cable types to accommodate flying leads or pre-wired field connections.

Product range

Migration made easy.

The migration process - our solutions at a glance

Scenario 1: PLC system was installed with PLC interface modules

In this case, only the PLC cable with proper connector and the PLC or DCS itself has to be replaced.

Scenario 2: Card solution (rack in place)

If in the new installation has enough space to add the rack of the new PLC or DCS without disassemble the old one. In this case, the adaptor card can be placed in the old PLC rack, while the new control system is located in a different cabinet/location. The adaptor card is provided with two connectors.

Scenario 3: Addcon solution

The Addcon system is a new system for migrating between PLCs. An adaptor is connected between the new PLC and the old PLC cables. Since no adapter chassis are required, migration can be performed very quickly, error-free and without additional space requirements.

Scenario 4: Bridge solution

The Bridge solution does not require any additional space in the control cabinet. The adapter chassis and bridge take the place of the old controller and combine the connections from the field devices to the new controller into one compact unit.

Services

White paper on migration solutions

In our white paper we have composed detailed information about the latest trends and solutions in the field of PLC migration. Find out what has proven itself in practice and which developments will bring your project forward.

Downloads

White paper on migration solutions

With Weidmüller PLC / DCS migration interfaces, there’s no need to make any changes to the field cabling, so this shortens the amount of time needed to upgrade the entire plant. Indeed, what used to be a PLC and DCS migration process that lasted a good few weeks is now an update that can be completed in just a few hours – including the system tests. Production facilities can return to operating as normal even after the briefest of downtimes. Request the free white paper and learn more about our solutions.

Select your downloads (0 selected)

Please select at least one download

Enter your contact credentials

* Required fields

Perfect complements

Consulting & Support

Do you have questions about our products and services or would you like an individual offer? Simply fill out contact form. Our employees will contact you as soon as possible.

* Required fields