Press Releases

Contact:

More Weidmüller

.

Select Languageenglish

Weidmüller’s "multi-stripax® PV": Practical, multi-functional tool

To facilitate precise preparation of cables and conductors utilised in the photovoltaic sector Weidmüller now proudly offers the practical "multi-stripax® PV", the multifunctional cutting and stripping tool.

 

Distinguishing characteristics of cables utilised in the photovoltaic/solar energy sector include very good UV, weather and temperature resistance. They have good notch and abrasion resistance properties, are free from halogens and flame retardant. Designed for longevity they are specifically fabricated and structured to meet the requirements demanded of photovoltaic applications over a long period of time. For example a strengthened outer sheathing is provided for some cable types to protect against mechanical influences. On the one hand a robust construction is necessary to ensure the PV system is able to function over many years, but on the other hand this presents a huge challenge in respect of precise cable preparation requirements. The tasks of "cutting and insulation stripping" of solar cables is relatively imprecise with the insulation stripping tools currently available on the market; what is more, only a limited range of cable types can be processed per set of blades. Weidmüller has taken a closer look at this problem and is now proud to present the new "multi-stripax® PV", a practical, multifunctional tool designed to precisely cut and strip the insulation of solar cables.

 

Utilising the "multi-stripax® PV" eliminates the need to swap tools or change blades and enables the user to precisely process the solar cables of the following manufacturers: ELDRA, ELDSOLAR®; Huber+Suhner, RADOX® SOLAR; LAPPKABEL, Oelflex® SOLAR; Leoni, BETAflam® 125 flex SOLAR; NEXANS, ENERGYFLEX® / ENERGYFLEX Plus and ARISTONCAVI NSGAFöU.

 

Very good cutting and insulation stripping results together with excellent repeat accuracy and a long service life are compelling arguments in favour of the "multi-stripax® PV". The special inserts precisely remove the cable insulation of 2.5 mm², 4 mm² and 6 mm² conductor cross-sections. The insulation stripping quality has been designed to meet the demanding requirements of industrial applications. Precise insulation stripping lengths from 2.3 mm – 30 mm is made possible by a length stop, adjustable in millimetre steps. The insulation stripping operation is simply repeated for applications requiring longer lengths of stripped insulation. The integrated cable cutter precisely cuts flexible core cables up to 6 mm² and single-core cables up to 2.5 mm². "multi-stripax® PV" is the first practical, multifunctional tool to speed up the work processes "cutting and insulation stripping", saving both time and money as a result.

 

Insulation stripping is the process of cutting through and removing cable insulation. To exclude the possibility of errors creeping in during this process and achieve reproducible good results requires high-quality insulation stripping tools. Such tools guarantee consistent results. The unique insulation stripping tool "multi-stripaxâ PV" is able to meet each and every challenge the market has to offer. The specially designed blade for these cables ensures a flawless insulation stripping result. Guide plates simplify correct positioning of the cable as well as prevent it from being damaged. The clamping jaws apply the requisite holding force to the cable during the insulation stripping process. Just a few work steps is all it takes to strip the cable of insulation. Cut the cable, insert the cable from the side and strip the insulation – job done!

 

The ergonomic design ensures working with "multi-stripax® PV" is fatigue free. Designed-in stability guarantees a long service life and high levels of reliability. This all means the "multi-stripax® PV" can be used outdoors without any restrictions.

 
 

topback

 

.