Industries & Applications

More Information

 

More Weidmüller

.

Select Languageenglish

PUSH IN – economically and ecologically convincing

SEVA Energie AG is a supplier of biogas block-type thermal power stations. Weidmüller supports SEVA Energie with the innovative PUSH IN connection technology. Here, all components are made from environmentally compatible material.

 

For SEVA Energie AG, economy and ecology are inseparably combined. Thermal power stations from SEVA are a gainful investment not only for their operator but also for the environment. Therefore, it is of utmost importance for SEVA that the components and solutions of their supplying partners are environmentally friendly. Other exceedingly important factors are the stability and reliability of all components as the average life-span of the thermal power stations is up to ten years – and this while reaching a twenty-four-seven availability.

 

All these characteristics required by SEVA are qualities of Weidmüller's PUSH IN connection technology. PUSH IN is one of the most secure connection technologies in the field of electrical connectivity. Furthermore, it can be intuitively connected and is suited to all applications in all industries. The prepared conductor is simply inserted into the clamping point and immediately guarantees a reliable, vibration-resistant and gas-tight connection. This connection outlives the life-span of a thermal power station without any problems.

 
 A technician from SEVA connects a PUSH IN terminal from Weidmüller on the mounting rail

A technician from SEVA connects a PUSH IN terminal from Weidmüller on the mounting rail

 

Besides this maximum stability and reliability, all material within the Weidmüller's innovative and comprehensive PUSH IN product range has been tested thoroughly according to the latest environmental guidelines. The material is absolutely consistent with the EU directive RoHS which specifies the restriction of potentially hazardous substances.

 

This way, Weidmüller has proven itself as an ideal partner for SEVA Energie AG. The company is very satisfied with the PUSH IN connection technology, which is innovative and environmentally friendly at the same time.

 

topback

 

.