- M12 cables with plastic nuts as a cost-efficient solution
more information |
.
Select Language
english
In some mechanical engineering applications, the proven M12 cables with nickel-plated M12 nuts cannot be used because the surroundings are too aggressive. As an alternative, cables with stainless-steel threaded rings are used here. As a cost-efficient solution, Weidmuller offers M12 cables with plastic nuts that match the dimensions of the standard metal nuts 1:1.
These M12 plastic nuts with protection class IP67 can withstand even the most adverse environmental conditions.
Plastic cable glands enable the use of M12 plug-type connectors in adverse environments that would oxidise cables with nickel-plated M12 nuts.
Protection class IP 67. Withstands even aggressive cleaning agents.
Economical alternative to stainless steel
The plastic nut corresponds to the dimensions of the metal nuts 1 to 1. Thus, no changes in handling are necessary.