Archive

Contact:

Weidmüller Interface

GmbH & Co. KG

Trade Press

Dipl.-Ing. Horst Kalla

P.O. Box 30 30

32720 Detmold

Germany

 

.

Select Languageenglish

Weidmüller FrontCom® Micro

Practical service interface for Ethernet and USB applications.

 

By adding the new service interface FrontCom® Micro Weidmüller is enhancing the FrontCom® family with a further practical product.

A compact design, IP65 ingress protection, a wealth of Ethernet and USB inserts in addition to STEADYTEC™ technology all ensure that the FrontCom® Micro is a secure and versatile service interface that facilitates simple access to the inner workings of the electrical cabinet.

 

Generally speaking, standardized interface ports such as RJ45 and USB are utilized to access the controls or PC in order to programme and set parameters of an installation.

These devices are installed on the inside of the electrical cabinet.

Consequently, users have to open the cabinet door to undertake service tasks. An opened cabinet door, however, also opens the door to risks.

 
 Weidmüller FrontCom® Micro

Weidmüller's FrontCom® Micro

 

The components are open to damaging environmental factors and unauthorized access. Weidmüller turned its attention to this problem and developed a stunningly simple and practical solution in the form of its FrontCom® Micro.

 

FrontCom® Micro simply enables simple access to the devices on the inside of the electrical cabinet. It avoids having to open the door of the electrical cabinet and all the risks that that entails. With FrontCom® Micro carrying out service work at the electrical cabinet is simple, fast and secure.

 

For high resolution photographs, please contact our trade press department (see contact information in left column). Download the full length press release as a PDF file by clicking on the link below.

 
 

topback

 

.